XIAO ESP32S3 SENSE - Arduino - I2S MIC init question

SUCCESS!

After some try-and-error, I have a working configuration!
I tested with a little Edge Impulse Studio AI Keyword Spotting App, it is WORKING OK!

The WORKING config shown below…
The following is a FULL CODE sample using the I2S MIC PDM config for use with XIAO ESP32S3 SENSE { After uploading, open the Serial Plotter to see the MIC output }:

#include <driver/i2s.h>

i2s_config_t i2s_config = {
    .mode                 = (i2s_mode_t)(I2S_MODE_MASTER | I2S_MODE_RX | I2S_MODE_PDM ),
    .sample_rate          = 16000U,
    .bits_per_sample      = I2S_BITS_PER_SAMPLE_16BIT,
    //.channel_format       = I2S_CHANNEL_FMT_ONLY_RIGHT,     // Also works
    .channel_format       = I2S_CHANNEL_FMT_ONLY_LEFT,
    //.communication_format = I2S_COMM_FORMAT_PCM,            // Also works
    .communication_format = I2S_COMM_FORMAT_I2S,
    .intr_alloc_flags     = ESP_INTR_FLAG_LEVEL1,
    .dma_buf_count        = 4,
    .dma_buf_len          = 1024,
    .use_apll             = false,
    .tx_desc_auto_clear   = false,
    .fixed_mclk           = 0
};
   
i2s_pin_config_t i2s_mic_pins = {
    .bck_io_num     = I2S_PIN_NO_CHANGE,
    .ws_io_num      = 42,
    .data_out_num   = I2S_PIN_NO_CHANGE,
    .data_in_num    = 41   
};

void setup() {
  Serial.begin(115200);
  
  // start up the I2S peripheral
  i2s_driver_install(I2S_NUM_0, &i2s_config, 0, NULL);
  i2s_set_pin(I2S_NUM_0, &i2s_mic_pins);
}

#define BUFFER_SIZE 512
int16_t raw_samples[BUFFER_SIZE];

void loop() {
  // read from the I2S device
  size_t bytes_read = 0;
  i2s_read(I2S_NUM_0, raw_samples, sizeof(int16_t) * BUFFER_SIZE, &bytes_read, portMAX_DELAY);
  int samples_read = bytes_read / sizeof(int16_t);
  
  for (int i = 0; i < samples_read; i++) {
    Serial.printf("%ld\n", raw_samples[i]);
  }
}

Edge Impulse Studio
Edge Impulse Studio does not yet support ESP32S3 officially, so, the NPU functions of the CHIP cannot be used yet (we need to disable NN [neural net] function calls in code)… but, at least, now I can use the generated (there) code to run on the XIAO ESP32S3 SENSE with minimalist changes/adaptations…
It is nice to be able to run some basic AI-MACHINE LEARNING stuff on the XIAO ESP32S3, even without the full benefit of the NPU functions on the CHIP…

Regards all,
Valter