Thank you! Yes, it does show up as a JTAG, with the instructions you provided. However, when I do update the driver, the only device that works is WinUsb Device, and when I do update it, it says it successfully installed it yet doesn’t change in the device manager nor is it included in the Arduino ports. I have also attempted rebooting and reseting it, but nothing seems to change. Should the USB Serial Device be an option?