XIAO_ESP32C6 Switching between builtin and external antenna

If the RF switch should be enabled whenever using WiFi (and not just the external antenna) it’s odd that the Seeed wiki doesn’t state it explicitly. I recall they only mention you should do it for the external antenna.

It would be good if Seed Studio released the final schematic (without crossed-out components) and positioned themselves about this.

I wanted to upgrade to the C6 from the S3, but the WiFi connectivity has proven to be very unstable (I don’t know if it’s a problem with the antenna configuration or something else).