XIAO_ESP32C6 Switching between builtin and external antenna

This is an interim report on some experiments with BLE regarding the effects of RF switch power on/off and antenna selection.
The conditions are as follows

  1. Receiver side turns on RF switch and uses an external antenna
  2. Transmitter side, RF switch is on or off, and an antenna is selected
  3. When sing an on-board antenna, an external antenna must be removed
  4. The distance is approximately 10 meters over a wall

The results are summarised in the graph below.
When RF switch is powered, an external antenna has about 10 dB advantage over an on-board antenna. When RF switch is not powered, an external antenna is about 10 dB smaller, while an on-board antenna is about 30 dB smaller.

Based on the “powered from input pins” hypothesis:
If an external antenna is selected on HIGH, it will drop by 10 dB, but appears to be working. On the other hand, when set to LOW and an on-board antenna is selected, it is 25 dB smaller, close to the data sheet isolation value of 30 dB.
This is just my hypothesis.