Try this:
// 8[dBm] * 4 = 32
esp_wifi_set_max_tx_power(32);
To explicitly use the on-board antenna.
#define RF_SW_PWR 3 // RF switch power pin
#define RF_PORT 14 // RF port select pin
// RF switch select default setting LOW:power on, LOW:built-in antenna
pinMode(RF_SW_PWR, OUTPUT);
digitalWrite(RF_SW_PWR, LOW); // LOW:power on
pinMode(RF_PORT, OUTPUT);
digitalWrite(RF_PORT, HIGH); // HIGH:external antenna