I have 2 XIAO ESP32C6 4" apart.
I am sending a broadcast using esp-now.
When receiving I am looping over the peers_table to display rssi.
In this example I am getting -67.
At this distance I expected better signal.
At 2’ it drops to -80
At 4’ it drops to -90
At 14’ it stops receiving data.
Do I just have to purchase external antennas to make this work more reliably at greater distances ?
The antennas must be properly facing each other.
To explicitly use the on-board antenna, try this
#define RF_SW_PWR 3 // RF switch power pin
#define RF_PORT 14 // RF port select pin
// RF switch select default setting LOW:power on, LOW:built-in antenna
pinMode(RF_SW_PWR, OUTPUT);
digitalWrite(RF_SW_PWR, LOW); // LOW:power on
pinMode(RF_PORT, OUTPUT);
digitalWrite(RF_PORT, HIGH); // HIGH:external antenna
The following can be used to change the output.
// N15, N12, N9, N6, N3, N0, P3, P6, P9, P12, P15, P18, P20
esp_ble_tx_power_set(ESP_BLE_PWR_TYPE_DEFAULT, ESP_PWR_LVL_N0);
The following links may also be helpful.
1 Like
Did you check your code in both sender and receiver sides?
Can esp_ble_tx_power_set be used even though I am not using bluetooth ? I am only using esp-now.
When I try to esp_ble_tx_power_set I get a core dump.
Try this:
// 8[dBm] * 4 = 32
esp_wifi_set_max_tx_power(32);
To explicitly use the on-board antenna.
#define RF_SW_PWR 3 // RF switch power pin
#define RF_PORT 14 // RF port select pin
// RF switch select default setting LOW:power on, LOW:built-in antenna
pinMode(RF_SW_PWR, OUTPUT);
digitalWrite(RF_SW_PWR, LOW); // LOW:power on
pinMode(RF_PORT, OUTPUT);
digitalWrite(RF_PORT, HIGH); // HIGH:external antenna
You do not need to use those defines if you write the code like this
pinMode(WIFI_ENABLE, OUTPUT);
digitalWrite(WIFI_ENABLE, LOW);
delay(100);
pinMode(WIFI_ANT_CONFIG, OUTPUT);
digitalWrite(WIFI_ANT_CONFIG, HIGH);
1 Like