Xiao esp32c3 - powering with 3.3v pin

Yes a very good forum, You see the caveat in the end"if your pants are full" loose translation on that if you do Hook it up this way,
Here is the Main Jists and I take NO credit for the findings.

Jens G. wrote:
 > The manufacturers usually do not provide any details because this 
mode of operation is not usually the norm and therefore the manufacturers 
save themselves the effort of 
specifying this in detail with all possible circumstances.

This is available on request if you buy enough of the components.

Basically, the operating case is uncritical if you consider a few points
noted:

* for bipolar voltage regulators (eg 7812) the output voltage
not be more than 6 V above the input voltage. Otherwise the
Output transistor. In the data sheets, a diode is usually
Output to input recommended, which limits the difference to 0.7 V.
This only applies to regulators that have more than 6 V at the output
With 5 V or 3.3 V this is not an issue, a 7805 does not need
Diode.

* For LDOs with MOSFETs, no significant current may flow through the
Backgate diode. Every MOSFET acts backwards as a diode, so does
the internal one. That means that nothing should be connected to the input that
draws current permanently. An electrolytic capacitor is OK, a complete circuit on the
next higher voltage level.

* The reset generator often looks at the input. That is, if the input is open
and output is externally powered, the reset pin is often activated. This disturbs
when flashing.
Of course, this only applies to LDOs with a reset pin or watchdog.

GL :slight_smile: PJ
:v: