XIAO ESP32C3 high power consumption and weird LED behavior

So, did some more measurements. The PPK2 did arrive in the meantime and shows some slightly different values.

  • Previous current measurement with uCurrent and DDM: ~218 uA
  • new with PPK2: ~245 uA

To estimate, which of the two might be “more correct”, I looked for some DDM with the ability to measure sub-mA ranges directly:

  • directly with current measuring functionality of 4.5 digit DDM at 2000 uA range: ~250 uA
  • directly with current measuring functionality of cheap 3.5 digit DDM at 2000 uA range: ~250 uA

So it seams that my uCurrent is a bit off, as the other measurements without the uCurrent show very similar values.

I did now as well probe the LED directly with the oscilloscope and got again ~24 Hz, but a clearly longer pulse duration of ~353 us, which was not visible in the current measurements with the uCurrent.

1 Like