apparently
I do not have I2S hardware to test
but check this link… some data copied below
The I²S bus consists of at least three lines:
Note
All lines can be attached to almost any pin and this change can occur even during operation.
- Bit clock line
- Officially “continuous serial clock (SCK)”. Typically written “bit clock (BCLK)”.
- In this library function parameter
sckPinor constantPIN_I2S_SCK.
- Word clock line
- Officially “word select (WS)”. Typically called “left-right clock (LRCLK)” or “frame sync (FS)”.
- 0 = Left channel, 1 = Right channel
- In this library function parameter
fsPinor constantPIN_I2S_FS.
- Data line
- Officially “serial data (SD)”, but can be called SDATA, SDIN, SDOUT, DACDAT, ADCDAT, etc.
- Unlike Arduino I2S with single data pin switching between input and output, in ESP core driver use separate data line for input and output.
- For backward compatibility, the shared data pin is
sdPinor constantPIN_I2S_SDwhen using simplex mode. - When using in duplex mode, there are two data lines:
- Output data line is called
outSdPinfor function parameter, or constantPIN_I2S_SD_OUT - Input data line is called
inSdPinfor function parameter, or constantPIN_I2S_SD_IN
- Output data line is called
Pin setup¶
Pins can be changed in two ways- 1st constants, 2nd functions.
Note
Shared data pin can be equal to any other data pin, but must not be equal to clock pin nor frame sync pin! Input and Output pins must not be equal, but one of them can be equal to shared data pin!
sckPin != fsPin != outSdPin != inSdPin
sckPin != fsPin != sdPin
By default, the pin numbers are defined in constants in the header file. You can redefine any of those constants before including I2S.h. This way the driver will use these new default values and you will not need to specify pins in your code. The constants and their default values are:
PIN_I2S_SCK14PIN_I2S_FS25PIN_I2S_SD26PIN_I2S_SD_OUT26PIN_I2S_SD_IN35
The second option to change pins is using the following functions. These functions can be called on either on initialized or uninitialized object.
setAllPins¶
Set all pins using given values in parameters. This is simply a wrapper of four functions mentioned above.
int setAllPins(int sckPin, int fsPin, int sdPin, int outSdPin, int inSdPin)
Set all pins to default i.e. take values from constants mentioned above. This simply calls the the function with the following constants.
PIN_I2S_SCK14PIN_I2S_FS25PIN_I2S_SD26PIN_I2S_SD_OUT26PIN_I2S_SD_IN35
int setAllPins()