XIAO-ESP32-S3 with ST7789 1.22" display

HI There,

SO post up the code you are trying to use, S3 correct So with it’s SPI and IC2 you need to define the pins explicitly with the interfaces selected “begin” Post upp the compiler output, First 3 lines and the last 12 -15 lines b4 the Upload. I can look.

Also have a look at the link in this thread , compare the output you get with the ones in that thread above. If you have an UNO also would be worth trying(learning) the difference :+1:

HTH
GL :slight_smile: PJ :v: