XIAO ESP32-C3 on bootloop when using Adafruit Neopixel library

Hi, PJ!

Thanks for your answer. I think the connections are correct, because:

  • It doesn’t matter if I power the neopixel strip from an outside power strip, the error persists
  • The connections should be allright, because I use the same wires as I use with an standard ESP32, and they work correctly on the ESP32.
  • Even if I completely disconnect the XIAO ESP32-C3 from the Neopixel Strip, the error persists. In an standard ESP32, it runs conrrectly both connected and disconnected from the strip. The program just sends data and doesn’t read from the neopixel strip.

I would like to know if the simple test program I transcribed on my second post just runs on an XIAO ESP32-C3 from somebody, not showing the error messages I see in serial console. If it happens that way, it may happen that my XIAO ESP32-C3 is defective and I have request a new one.

Regards!