XIAO esp32-c3 No Code Execution

Hello,
I’ve unchecked the show compatible hardware checkbox i’m still unable to find the USB driver,

I’ve checked through the options, Perhaps the correct driver is not installed?

Anyhow i’ve tried booting the board with the strapping pin GPIO 8/9 as @ahsrabrifat requested and it worked!
The code runs normally now,

I think the issue was that the chip got stuck in download mode and was never booting into SPI? mode to actually run the code

Thank you so much for your help and support

I fixed it by pulling up GPIO 9

1 Like