Hi Timk5000,
I tried this with a new unit just received, Seems to work OK.
HTH
GL:-)
PJ
// Test code to get chip ID and STUFF
uint32_t chipId = 0;
int Vibration_signal = B10;
int Sensor_State = 1;
void setup() {
Serial.begin(9600);
delay (2000);
for(int i=0; i<17; i=i+8) {
chipId |= ((ESP.getEfuseMac() >> (40 - i)) & 0xff) << i;
}
pinMode(Vibration_signal,INPUT);
Serial.begin(9600);
Serial.printf("ESP32 Chip model = %s Rev %d\n", ESP.getChipModel(), ESP.getChipRevision());
Serial.printf("This chip has %d cores\n", ESP.getChipCores());
Serial.print("Chip ID: "); Serial.println(chipId);
}
void loop() {
Serial.print("Vibration Status: ");
Sensor_State = digitalRead(Vibration_signal);
if (Sensor_State ==1){
Serial.println("Machine Running");
}
else {
Serial.println("Machine Stopped");
}
delay(3000);
}
I get this Output AOK
ESP-ROM:esp32c3-api1-20210207
Build:Feb 7 2021
rst:0x15 (USB_UART_CHIP_RESET),boot:0x8 (SPI_FAST_FLASH_BOOT)
Saved PC:0x4200ec40
SPIWP:0xee
mode:DIO, clock div:1
load:0x3fcd5810,len:0x438
load:0x403cc710,len:0x91c
load:0x403ce710,len:0x25b0
entry 0x403cc710
ESP32 Chip model = ESP32-C3 Rev 3
This chip has 1 cores
Chip ID: 4196588
Vibration Status: Machine Stopped
Vibration Status: Machine Stopped
Vibration Status: Machine Stopped
Here is the Build Log info, just FYI
FQBN: esp32:esp32:deneyapkartg
Using board 'deneyapkartg' from platform in folder: C:\Users\Dude\AppData\Local\Arduino15\packages\esp32\hardware\esp32\2.0.8
Using core 'esp32' from platform in folder: C:\Users\Dude\AppData\Local\Arduino15\packages\esp32\hardware\esp32\2.0.8
"C:\\Users\\Dude\\AppData\\Local\\Temp\\arduino\\sketches\\B0BFC6AD928EE0E6D13E03AD142A923F/GetChipID.ino.bin" "C:\\Users\\Dude\\AppData\\Local\\Temp\\arduino\\sketches\\B0BFC6AD928EE0E6D13E03AD142A923F/GetChipID.ino.elf"
esptool.py v4.5.1
Creating esp32c3 image...
Merged 2 ELF sections
Successfully created esp32c3 image.
"C:\\Users\\Dude\\AppData\\Local\\Arduino15\\packages\\esp32\\hardware\\esp32\\2.0.8/tools/gen_esp32part.exe" -q "C:\\Users\\Dude\\AppData\\Local\\Temp\\arduino\\sketches\\B0BFC6AD928EE0E6D13E03AD142A923F/partitions.csv" "C:\\Users\\Dude\\AppData\\Local\\Temp\\arduino\\sketches\\B0BFC6AD928EE0E6D13E03AD142A923F/GetChipID.ino.partitions.bin"
cmd /c if exist "C:\\Users\\Dude\\AppData\\Local\\Temp\\arduino\\sketches\\B0BFC6AD928EE0E6D13E03AD142A923F\\libraries\\Insights" "C:\\Users\\Dude\\AppData\\Local\\Arduino15\\packages\\esp32\\hardware\\esp32\\2.0.8/tools/gen_insights_package.exe" "C:\\Users\\Dude\\AppData\\Local\\Temp\\arduino\\sketches\\B0BFC6AD928EE0E6D13E03AD142A923F" GetChipID.ino "D:\\Arduino_projects\\GetChipID"
cmd /c IF 0==1 COPY /y "C:\\Users\\Dude\\AppData\\Local\\Arduino15\\packages\\esp32\\tools\\openocd-esp32\\v0.11.0-esp32-20221026\\share\\openocd\\scripts\\board\\esp32c3-builtin.cfg" "D:\\Arduino_projects\\GetChipID\\debug.cfg"
cmd /c IF 0==1 COPY /y "C:\\Users\\Dude\\AppData\\Local\\Arduino15\\packages\\esp32\\hardware\\esp32\\2.0.8\\tools\\ide-debug\\esp32c3.json" "D:\\Arduino_projects\\GetChipID\\debug_custom.json"
cmd /c IF 0==1 COPY /y "C:\\Users\\Dude\\AppData\\Local\\Arduino15\\packages\\esp32\\hardware\\esp32\\2.0.8\\tools\\ide-debug\\svd\\esp32c3.svd" "D:\\Arduino_projects\\GetChipID\\debug.svd"
"C:\\Users\\Dude\\AppData\\Local\\Arduino15\\packages\\esp32\\tools\\riscv32-esp-elf-gcc\\esp-2021r2-patch5-8.4.0/bin/riscv32-esp-elf-size" -A "C:\\Users\\Dude\\AppData\\Local\\Temp\\arduino\\sketches\\B0BFC6AD928EE0E6D13E03AD142A923F/GetChipID.ino.elf"
Sketch uses 230134 bytes (17%) of program storage space. Maximum is 1310720 bytes.
Global variables use 15856 bytes (4%) of dynamic memory, leaving 311824 bytes for local variables. Maximum is 327680 bytes.
(Trucated_PJG)...
"C:\Users\Dude\AppData\Local\Arduino15\packages\esp32\tools\esptool_py\4.5.1/esptool.exe" --chip esp32c3 --port "COM23" --baud 921600 --before default_reset --after hard_reset write_flash -z --flash_mode dio --flash_freq 80m --flash_size 4MB 0x0 "C:\Users\Dude\AppData\Local\Temp\arduino\sketches\B0BFC6AD928EE0E6D13E03AD142A923F/GetChipID.ino.bootloader.bin" 0x8000 "C:\Users\Dude\AppData\Local\Temp\arduino\sketches\B0BFC6AD928EE0E6D13E03AD142A923F/GetChipID.ino.partitions.bin" 0xe000 "C:\Users\Dude\AppData\Local\Arduino15\packages\esp32\hardware\esp32\2.0.8/tools/partitions/boot_app0.bin" 0x10000 "C:\Users\Dude\AppData\Local\Temp\arduino\sketches\B0BFC6AD928EE0E6D13E03AD142A923F/GetChipID.ino.bin"
esptool.py v4.5.1
Serial port COM23
Connecting...
Chip is ESP32-C3 (revision v0.3)
Features: WiFi, BLE
Crystal is 40MHz
MAC: a0:76:4e:40:08:ec
Uploading stub...
Running stub...
Stub running...
Changing baud rate to 921600
Changed.
Configuring flash size...
Flash will be erased from 0x00000000 to 0x00003fff...
Flash will be erased from 0x00008000 to 0x00008fff...
Flash will be erased from 0x0000e000 to 0x0000ffff...
Flash will be erased from 0x00010000 to 0x0004afff...
Compressed 13152 bytes to 9473...
Writing at 0x00000000... (100 %)
Wrote 13152 bytes (9473 compressed) at 0x00000000 in 0.2 seconds (effective 448.9 kbit/s)...
Hash of data verified.
Compressed 3072 bytes to 146...
Writing at 0x00008000... (100 %)
Wrote 3072 bytes (146 compressed) at 0x00008000 in 0.0 seconds (effective 636.2 kbit/s)...
Hash of data verified.
Compressed 8192 bytes to 47...
Writing at 0x0000e000... (100 %)
Wrote 8192 bytes (47 compressed) at 0x0000e000 in 0.1 seconds (effective 639.7 kbit/s)...
Hash of data verified.
Compressed 241664 bytes to 135200...
Writing at 0x00010000... (11 %)
Writing at 0x0001ab45... (22 %)
Writing at 0x000226cd... (33 %)
Writing at 0x000284d7... (44 %)
Writing at 0x0002e661... (55 %)
Writing at 0x0003464d... (66 %)
Writing at 0x0003c2a9... (77 %)
Writing at 0x00042ff8... (88 %)
Writing at 0x000495a3... (100 %)
Wrote 241664 bytes (135200 compressed) at 0x00010000 in 2.1 seconds (effective 923.7 kbit/s)...
Hash of data verified.
Leaving...
Hard resetting via RTS pin...