XIAO ESP32-C3 button don't work

Hi,
Thanks for the code. I set your code, push the button many time and I get this


Power ON 
 
Test program compiled on Nov  4 2023 at 13:15:03

Processor came out of reset.

On the screen, I read POWER ON then Loop and HIGH. It never change.

I must make one change , I replace

U8X8_SSD1306_128X64_NONAME_HW_I2C u8x8(/* clock=*/PIN_WIRE_SCL, /* data=*/PIN_WIRE_SDA, /* reset=*/U8X8_PIN_NONE);  // OLEDs without Reset of the Display

by

U8X8_SSD1306_128X64_NONAME_HW_I2C u8x8(U8X8_PIN_NONE); 

Because first line don’t compile (PIN_WIRE_SCL is not recognize) , and I see this solution on a forum.

Do you think the issue can come from a library ?
I use seeduino and arduino from years but it is my first time with an esp32. There is somthing special to do to have the entry ?

Thanks for your help !