Xiao bricked and not responding anymore

Just received my J-Link Programmer and downloaded SEGGER JFlash

But when trying Target->connect I get following error:

  • InitTarget() end
  • RESET (pin 15) high, but should be low. Please check target hardware.

Target->Programming gives following error:

Auto programming target (8192 bytes, 1 range) …

  • Connecting …
  • ERROR: Failed to connect.
    Could not establish a connection to target.
  • ERROR: Could not auto program target, not connected

I connected from JTAG
pin 7 → XIAO SWDIO
pin 9 → XIAO SWDCLK
pin 15 → XIAO RESET
pin 4 → XIAO GND

Plugged XIAO into USB for power