XIAO BLE wont compile ArduinoBLE- Arduino IDE

I have the same versions, the code:

#include <ArduinoBLE.h>

BLEService ledService("19B10000-E8F2-537E-4F6C-D104768A1214"); // Bluetooth® Low Energy LED Service

// Bluetooth® Low Energy LED Switch Characteristic - custom 128-bit UUID, read and writable by central
BLEByteCharacteristic switchCharacteristic("19B10001-E8F2-537E-4F6C-D104768A1214", BLERead | BLEWrite);

const int ledPin = LED_BUILTIN; // pin to use for the LED

void setup() {
  Serial.begin(9600);
  while (!Serial);

  // set LED pin to output mode
  pinMode(ledPin, OUTPUT);

etc.

Does not compile for Seeed nRF52 (no embedded ml) .

WARNING: library ArduinoBLE claims to run on samd, megaavr, mbed, apollo3, mbed_nano, mbed_portenta, mbed_nicla, esp32, mbed_giga, renesas, renesas_portenta, mbed_opta, renesas_uno architecture(s) and may be incompatible with your current board which runs on nrf52 architecture(s).

Is there any analogous tutorial for Adafruit Bluefruit?