XIAO BLE (Sense) bootloader bricked, how to restore it?

I was able to unbrick my XIAO BLE sense with OpenOCD using a raspberry pi as SWD debugger / programmer.

I just set up a fresh Raspberry PI OS on a Raspberry PI Zero W, and installed openocd (“sudo apt install openocd”), wired the XIAO BLE sense to the Raspberry PI (see below), and executed the following command:

sudo openocd -f interface/raspberrypi-native.cfg -c “transport select swd” -f target/nrf52.cfg -c init -c “reset init” -c halt -c “nrf5 mass_erase” -c “program Seeed_XIAO_nRF52840_Sense_bootloader-0.6.1_s140_7.3.0.hex verify” -c reset -c exit

The connections between Raspberry PI and the XIAO ble sense were made as follows:

  • GPIO 11 (header pin number 23) – TP3 (SWDCLK)
  • GPIO 25 (header pin number 22) – TP5 (SWDIO)
  • any of the 3.3V pins from the Raspberry PI – 3.3V pin of the XIAO
  • any of the GND pins from the Raspberry PI – GND pin of the XIAO

Took only seconds (ok needed a few moments to set everything up) and worked like a charm.

Thanks a lot, and take care when fiddling around with the flash memory. :wink: