XIAO 52840 Sense + Grove Shield - Battery Monitoring?

The Grove Shield battery is not connected to the XIAO port, so I don’t think it is possible to monitor the battery voltage. If you want to monitor it on XIAO, you need to divide the battery voltage appropriately and connect it to the port.
PIN_VBAT can read the battery voltage connected to the pad on the back of the XIAO nRF52840.

1 Like