Hi George, There are two antennae as the device is capable of 2x2 MIMO. So it has the option of using both antennae for Wi-Fi. So ANT1 is used for Wi-Fi and Bluetooth and ANT2 is used for the second Wi–Fi channel for MIMO. You can use on board antenna as well without the external antennas. you also can use one external antenna.please refer to schematic page 11 for the antennas. <LINK_TEXT text=“https://github.com/SeeedDocument/Beagle … 160314.pdf”>https://github.com/SeeedDocument/BeagleBone_Green_Wireless/tree/master/resources/BeagleBone_Green%20Wireless_V1.0_SCH_20160314.pdf</LINK_TEXT>
here is the wl1835mod datasheet. http://www.ti.com/lit/ds/symlink/wl1835mod.pdf
Seeed techsupport team
Bill