Apologies for responding to an old thread, but I wanted to add a possible solution in case anyone is reading this.
As per @Baozhu 's post here (Using Wio Terminal microphone with Edge Impulse), the internal mic is only configured (in hardware) to measure sound levels rather than actually record audio. To get around this, I was able to connect an electret microphone (with amplifier) to pin 13 (ADC0, PB08).
Here is an example that will read 1 second of audio and print it to the console in comma-separated value format (you can copy and paste these values into Python code to graph with Matplotlib or play the sound). It will only do this once on reboot.
// Use SAMD51's DMAC to read from microphone connected to PB08 (ADC0/AIN2)
// From: https://forum.arduino.cc/index.php?topic=685347.0
// and https://forum.arduino.cc/index.php?topic=709104.0
// Settings
#define DEBUG 1
enum { ADC_BUF_LEN = 1600 };
enum { AUDIO_BUF_LEN = ADC_BUF_LEN * 10 };
#if DEBUG
static const int debug_pin = 1; // Toggles each DAC ISR
#endif
// Structs
typedef struct // DMAC descriptor structure
{
uint16_t btctrl;
uint16_t btcnt;
uint32_t srcaddr;
uint32_t dstaddr;
uint32_t descaddr;
} dmacdescriptor ;
// Globals
volatile uint8_t recording = 0;
volatile boolean results0Ready = false;
volatile boolean results1Ready = false;
uint16_t adc_buf_0[ADC_BUF_LEN]; // ADC results array 0
uint16_t adc_buf_1[ADC_BUF_LEN]; // ADC results array 1
int16_t audio_buf[AUDIO_BUF_LEN]; // Big buffer for testing
volatile dmacdescriptor wrb[DMAC_CH_NUM] __attribute__ ((aligned (16))); // Write-back DMAC descriptors
dmacdescriptor descriptor_section[DMAC_CH_NUM] __attribute__ ((aligned (16))); // DMAC channel descriptors
dmacdescriptor descriptor __attribute__ ((aligned (16))); // Place holder descriptor
/*******************************************************************************
* Interrupt Service Routines (ISRs)
*/
// Called from ISR to copy double buffer contents
static void audio_rec_callback(uint16_t *buf, uint32_t buf_len) {
static uint32_t idx = 0;
// If recording flag is set, copy contents of ADC buffer to audio buffer
if (recording) {
for (int i = 0; i < buf_len; i++) {
// Convert 12-bit unsigned ADC value to 16-bit PCM (signed) audio value
audio_buf[idx] = ((int16_t)buf[i] - 2048) * 16;
// Increment big buffer pointer. If it reaches max, stop recording
idx++;
if (idx >= AUDIO_BUF_LEN) {
recording = 0;
idx = 0;
}
}
}
}
// Interrupt handler for DMAC channel 0
void DMAC_0_Handler() {
static uint8_t count = 0;
static uint16_t idx = 0;
// Check if DMAC channel 0 has been suspended (SUSP)
if (DMAC->Channel[0].CHINTFLAG.bit.SUSP) {
// Debug: make pin high before copying buffer
#if DEBUG
digitalWrite(debug_pin, HIGH);
#endif
// Restart DMAC on channel 0 and clear SUSP interrupt flag
DMAC->Channel[0].CHCTRLB.reg = DMAC_CHCTRLB_CMD_RESUME;
DMAC->Channel[0].CHINTFLAG.bit.SUSP = 1;
// See which buffer has filled up, and dump results into large buffer
if (count) {
audio_rec_callback(adc_buf_0, ADC_BUF_LEN);
} else {
audio_rec_callback(adc_buf_1, ADC_BUF_LEN);
}
// Flip to next buffer
count = (count + 1) % 2;
// Debug: make pin low after copying buffer
#if DEBUG
digitalWrite(debug_pin, LOW);
#endif
}
}
/*******************************************************************************
* Functions
*/
// Configure DMA to sample from ADC at regular interval
// I'm sorry everything is hardcoded. I don't have time to make a library.
// Adafruit_ZeroDMA may work--I haven't tried it.
void config_dma_adc() {
// Configure DMA to sample from ADC at a regular interval (triggered by timer/counter)
DMAC->BASEADDR.reg = (uint32_t)descriptor_section; // Specify the location of the descriptors
DMAC->WRBADDR.reg = (uint32_t)wrb; // Specify the location of the write back descriptors
DMAC->CTRL.reg = DMAC_CTRL_DMAENABLE | DMAC_CTRL_LVLEN(0xf); // Enable the DMAC peripheral
DMAC->Channel[0].CHCTRLA.reg = DMAC_CHCTRLA_TRIGSRC(TC5_DMAC_ID_OVF) | // Set DMAC to trigger on TC5 timer overflow
DMAC_CHCTRLA_TRIGACT_BURST; // DMAC burst transfer
descriptor.descaddr = (uint32_t)&descriptor_section[1]; // Set up a circular descriptor
descriptor.srcaddr = (uint32_t)&ADC0->RESULT.reg; // Take the result from the ADC0 RESULT register
descriptor.dstaddr = (uint32_t)adc_buf_0 + sizeof(uint16_t) * ADC_BUF_LEN; // Place it in the adc_buf_0 array
descriptor.btcnt = ADC_BUF_LEN; // Beat count
descriptor.btctrl = DMAC_BTCTRL_BEATSIZE_HWORD | // Beat size is HWORD (16-bits)
DMAC_BTCTRL_DSTINC | // Increment the destination address
DMAC_BTCTRL_VALID | // Descriptor is valid
DMAC_BTCTRL_BLOCKACT_SUSPEND; // Suspend DMAC channel 0 after block transfer
memcpy(&descriptor_section[0], &descriptor, sizeof(descriptor)); // Copy the descriptor to the descriptor section
descriptor.descaddr = (uint32_t)&descriptor_section[0]; // Set up a circular descriptor
descriptor.srcaddr = (uint32_t)&ADC0->RESULT.reg; // Take the result from the ADC0 RESULT register
descriptor.dstaddr = (uint32_t)adc_buf_1 + sizeof(uint16_t) * ADC_BUF_LEN; // Place it in the adc_buf_1 array
descriptor.btcnt = ADC_BUF_LEN; // Beat count
descriptor.btctrl = DMAC_BTCTRL_BEATSIZE_HWORD | // Beat size is HWORD (16-bits)
DMAC_BTCTRL_DSTINC | // Increment the destination address
DMAC_BTCTRL_VALID | // Descriptor is valid
DMAC_BTCTRL_BLOCKACT_SUSPEND; // Suspend DMAC channel 0 after block transfer
memcpy(&descriptor_section[1], &descriptor, sizeof(descriptor)); // Copy the descriptor to the descriptor section
// Configure NVIC
NVIC_SetPriority(DMAC_0_IRQn, 0); // Set the Nested Vector Interrupt Controller (NVIC) priority for DMAC0 to 0 (highest)
NVIC_EnableIRQ(DMAC_0_IRQn); // Connect DMAC0 to Nested Vector Interrupt Controller (NVIC)
// Activate the suspend (SUSP) interrupt on DMAC channel 0
DMAC->Channel[0].CHINTENSET.reg = DMAC_CHINTENSET_SUSP;
// Configure ADC
ADC0->INPUTCTRL.bit.MUXPOS = ADC_INPUTCTRL_MUXPOS_AIN2_Val; // Set the analog input to ADC0/AIN2 (PB08 - A4 on Metro M4)
while(ADC0->SYNCBUSY.bit.INPUTCTRL); // Wait for synchronization
ADC0->SAMPCTRL.bit.SAMPLEN = 0x00; // Set max Sampling Time Length to half divided ADC clock pulse (2.66us)
while(ADC0->SYNCBUSY.bit.SAMPCTRL); // Wait for synchronization
ADC0->CTRLA.reg = ADC_CTRLA_PRESCALER_DIV128; // Divide Clock ADC GCLK by 128 (48MHz/128 = 375kHz)
ADC0->CTRLB.reg = ADC_CTRLB_RESSEL_12BIT | // Set ADC resolution to 12 bits
ADC_CTRLB_FREERUN; // Set ADC to free run mode
while(ADC0->SYNCBUSY.bit.CTRLB); // Wait for synchronization
ADC0->CTRLA.bit.ENABLE = 1; // Enable the ADC
while(ADC0->SYNCBUSY.bit.ENABLE); // Wait for synchronization
ADC0->SWTRIG.bit.START = 1; // Initiate a software trigger to start an ADC conversion
while(ADC0->SYNCBUSY.bit.SWTRIG); // Wait for synchronization
// Enable DMA
DMAC->Channel[0].CHCTRLA.bit.ENABLE = 1; // Enable DMAC ADC on channel 1
// Configure Timer/Counter 5
GCLK->PCHCTRL[TC5_GCLK_ID].reg = GCLK_PCHCTRL_CHEN | // Enable perhipheral channel for TC5
GCLK_PCHCTRL_GEN_GCLK1; // Connect generic clock 0 at 48MHz
TC5->COUNT16.WAVE.reg = TC_WAVE_WAVEGEN_MFRQ; // Set TC5 to Match Frequency (MFRQ) mode
TC5->COUNT16.CC[0].reg = 3000 - 1; // Set the trigger to 16 kHz: (4Mhz / 16000) - 1
while (TC5->COUNT16.SYNCBUSY.bit.CC0); // Wait for synchronization
// Start Timer/Counter 5
TC5->COUNT16.CTRLA.bit.ENABLE = 1; // Enable the TC5 timer
while (TC5->COUNT16.SYNCBUSY.bit.ENABLE); // Wait for synchronization
}
/*******************************************************************************
* Main
*/
void setup() {
// Configure pin to toggle on DMA interrupt
#if DEBUG
pinMode(debug_pin, OUTPUT);
#endif
// Configure serial port
Serial.begin(115200);
// Configure DMA to sample from ADC at 16kHz
config_dma_adc();
// TEST: record for 1 second, print results in CSV
// Wait a second, start recording
while(!Serial);
delay(1000);
Serial.println("Recording...");
recording = 1;
// Wait for recording to be done, print results
while (recording);
for (int i = 0; i < AUDIO_BUF_LEN; i++) {
Serial.print(audio_buf[i]);
if (i < AUDIO_BUF_LEN - 1) {
Serial.print(", ");
}
}
Serial.println();
}
void loop()
{
delay(1000);
}