WIO Terminal blank screen

Hi folks- I’m having a similar issue with my new Wio Terminal for a hobby project (building a squirrel squirter that recognizes squirrels and shoots them with a water gun). I used my MacBook to flash the Wio to RTL8720 but it just displays “Burn RTL8720fw” and I’m unable to upload a sketch.

Instead I get the error message pasted below. I’d really appreciate any help/guidance that the community has to offer. (I also posted this q on Discord; hoping I’m not spamming the community!). THANK YOU!

Arduino: 1.8.19 (Mac OS X), Board: “Seeeduino Wio Terminal, Master, Enabled, 120 MHz (standard), Small (-Os) (standard), 50 MHz (standard), Arduino, Off, On”
Sketch uses 57368 bytes (11%) of program storage space. Maximum is 507904 bytes.
java.io.IOException: Cannot run program “/Users/oliver/Library/Arduino15/packages/Seeeduino/tools/bossac/1.8.0-48-gb176eee/bossac”: error=13, Permission denied