Wio LTE (4G) / I2C_LED Display

Hey,

jep, seems like they have edited this page in the last three years sometime…

If you check this readme in the WIO LTE repository from seeed there is a basic description about how to upgrade the firmware: https://github.com/SeeedDocument/Wio_LTE#software-updates

I’m not sure if it’s a good idea to use the firmware provided by the hardware manufacturers instead of the published firmware from seeed provided here: http://www.espruino.com/binaries/ (I think the one to use are the espruino_#v##_Wio_LTE.bin ones, the latest seems to be espruino_2v09_Wio_LTE.bin, uploaded 2021-04-19)

Hope this helps you a bit

Edit: nearly forgot that back then I created an issue regarding to the firmware flashing process, there is a litte bit more information about how I was able to set the board in DFU mode on a Windows PC: https://github.com/SeeedDocument/Wio_LTE/issues/1

1 Like