That sucks. They’re surface mount, too. Tricky for me to replace, even if we decide on a suitable replacement.
(I assume we’re talking about D5 in this image…)
The FPGA has internal diodes or the FPGA is 3.3V and we’re hitting it with 5V?
Is there a suitable non-surface-mount (ie. easy to solder) diode I could put across the input connector for ESD protection? That way I could remove the internal one…
If not I might think about removing it. I’m not a very ESD-prone person (touch wood) and the contacts on the quad/probe are reasonably hard to touch in normal use.