Hi,
at the moment we are using the Banana Pi M2 Berry.
It doesnt even give us the possibility to change the resolution. The Native
resolution there is 1280 x 720 and can’t be changed.
When i connect the Display to a Computer, then i can change the resolution.
There it is showing me the native resolution is 1024 x 600, but i still can
choose 1280 x 720.