Hi,
WJOIN command is only valid when the module joins the wireless network as STA or create a wireless network as an access point (AP). If the current network mode is adhoc, and no specified SSID network can be detected, the module will automatically create a new network. If it is already networking, then the network connection information will be directly returned.