Shouldn’t be a problem if nothing is connected to the pins I guess?
Thanks for investigating, that checks out! I modified my example sketch to verify if I can use pins 4-10 as long as I don’t use more than 4 pins in total - and I can!
Unfortunately I don’t understand what that means, could you elaborate? I tried running your example but only got an error from TinyUSB telling me that the board (Seeed XIAO BLE Sense - nRF52840) is not supported.
Thanks for pointing me to this. As @electry suggested, I opted for an IC not manufactured by Adafruit, as I can get 5 for the same price on AliExpress.
I appreciate the input from everyone! To sum up:
It seems to not be possible to output more than 4 PWM signals due to hardware limitations. To work around that, either generate the PWM signal using software or use an external IC like the PCA9685.