Unboxing-Wio-Tracker-L1-Pro

Package just arrived by DHL… cant wait to get it charged up!
Keep looking for test results


Hi there,

Oh’ SNAP :hand_with_index_finger_and_thumb_crossed: , Crackle :firecracker:and POP :exploding_head: that looks good , WOW!

You got a angle your working for it?
I may throw down some shekels for a 10" tablet for a Meshtastic app runner and a few other SDR lightweight apps & projects. My Mesh node has bee up a long time and folks are messaging it often , but it is too dam small to read the screen easy and I ain’t breaking out the phone to dork around.

GL :slight_smile: PJ :v:

the phone is the way to go… but a tablet will work too… i just ran a mission with it and practaced with the drone… problem is it is so flat around here

I set the range test to ping every minute… then get my stopwatch going on the phone… that way i can countdown to incoming ping… pretty cool way to check signal… also i found a website that shows in red cloud areas on the map that should be line of sight

gps is really wide on these other devices… T-1000 can tell i am in the house… just not which room

1 Like

Hello community!

I hope you can help me with the Wio Tracker L1 Lite. I’ve been working with this board and need specific information about the pin configuration that I haven’t been able to find in the publicly available documentation.

Specifically, I’m looking to know which nRF52840 GPIO pins are connected to:

  1. L76K GPS module (UART communication pins, control, etc.)
  2. SX1262 LoRa chip (SPI, control, interrupt pins, etc.)
  3. Other critical system signals
    I’ve tried:**
  • Reviewed official Seeed Studio documentation
  • Consulted Meshtastic wiki
  • Explored firmware repository on GitHub
  • Can’t find detailed schematic or specific pinout

Does anyone have:

  • The complete schematic of the board?
  • technical documentation?
  • Source code where these pins are specifically defined?

Any clue, link, or contact would be greatly appreciated! :pray:

good question… I have sent a message to my guy