have you tried the direct connect , and download Ublox, like the demo I posted with Air530 GPS, same thing should work according to this info on sales page.
About this item
- How to use the GPS module better, the link is obtained in the Product guides and documents, please download it before use
- Note: Please use the GT-U7 GPS module in an open place, the LED will flash after the satellite signal is found. Bad weather and indoor use will affect the accuracy of positioning
- GPS baud needs to be set to 9600 instead of 4800; PPS pin is not needed unless using the GPS to drive a hardware high precision clock; GT-U7 main module GPS module using the original UBLOX 7th generation chip, Software is compatible with NEO-6M. GT-U7 module, with high sensitivity, low power consumption, miniaturization, its extremely high tracking sensitivity greatly expanded its positioning of the coverage
- With a USB interface, you can directly use the phone data cable on the computer point of view positioning effect; With IPEX antenna interface, the default distribution of active antenna, can be quickly positioned
- USB directly connected to the computer, That is, with the host computer-owned serial port function, no need for external serial module, send IPX interface active antenna
HTH
GL PJ