Unable to backup reComputer Industrial J4011 on Jetpack 5.1.1

I have just now also tried using the backup and restore script in this repo: GitHub - Seeed-Studio/Linux_for_Tegra: Seeed Jetson reComputer && reServer default Image source code.šŸŽ šŸŽ šŸŽ, specifically I checked out branch r35.3.1.

Unfortunately this also fails, albeit with a slightly different error:

Save initrd flashing command parameters to /home/nx/flash/seeed_l4t/Linux_for_Tegra-r35.3.1/tools/kernel_flash/initrdflashparam.txt
/tmp/tmp.5qku8cwBXw ~/flash/seeed_l4t/Linux_for_Tegra-r35.3.1
writing boot image config in bootimg.cfg
extracting kernel in zImage
extracting ramdisk in initrd.img
/tmp/tmp.5qku8cwBXw/initrd /tmp/tmp.5qku8cwBXw ~/flash/seeed_l4t/Linux_for_Tegra-r35.3.1
55735 blocks
cp: cannot stat '/home/nx/flash/seeed_l4t/Linux_for_Tegra-r35.3.1/rootfs/lib/modules/5.10.104-tegra/kernel/drivers/mtd': No such file or directory
Cleaning up...

The entire log can be found in here:
seeed_github_l4t_log.zip (12.8 KB)