The battery charge issue

Thanks for your help.

The STM chip does see the voltage changes. When plugged into the USB port, the charge indicator goes green.
I measured the voltage at R51&R52 bridge, it’s exactly half of the input voltage. In my case, with battery voltage at 3.9v, I measured only 2.6v on top of the R52, thus it’s only 1.3v at the Vbat point. So the STM thinks battery is low for obvious reason.

The voltage at the on/off switch is only 2.6v. The voltage of the battery is 3.9v. So something is lost in between.

Looking at the schematic, I don’t understand why there is an X betwen pin 3 of U19 and the switch? Does that mean pin 3 is not connected?

If pin 3 is not connected then the voltage is passed from the battery solely through the diode inside U19. Is it a Schottky diode or is it a zener diode? I think it should be a Schottky diode. So maybe U19 is dead in my board. If I make a jumper between the switch and the battery, the quad indicates it’s 50% charged.

Could anyone please measure the voltage at the middle pin of your quad’s switch?

Thanks very much

-Thanh