(TECH) Upgrading/Flashing firmware without Windows

Hi!
Actually, I exactly talked about “main firmware”, which is closed RTOS, and, @dbelam already noticed me about existence of suitable API function, but it is a bin unclear, what actually should be used to flash:
API documentation says

But “SEEED02A_DEMO_BB.cfg” file in FirmwareUpdater directory, which is, as far as I understood wiki article about reflashing, used to flash RePhone by FirmwareUpdater, has a mention of “SEEED02A_DEMO_BOOTLOADER_V005_MT2502_MAUI_11CW1418SP5_W15_19.bin” (7Kb file), but not of file exactly named “image.bin”, which is there too, and has a size of 4.7Mb.

So, for now I just curious, what of that files is RePhone’s firmware. Or, even, if “image.bin” is RePhone firmware, or some general LinkIt Device’s :wink: