Support Thread for Seeeduino

I seem to be having problems with connecting to my seeeduino via usb.

I can connect to it but not consistently, approx 9/10 times I get:

[ 3581.747908] usb 1-2: new full speed USB device using uhci_hcd and address 97
[ 3581.869529] usb 1-2: device descriptor read/64, error -71
[ 3582.088561] usb 1-2: device descriptor read/64, error -71

so I have to pull the cable out and try again…

I’m running ubuntu on an eepc, usb ports work fine for other peripherals. Furthermore, the cable I’m using with fine with my phone, so both of those can be ruled out.

Is this normal behavior or am I doing something wrong?