Super Ping for Due

Ooops found and squashed a few bugs.[code]

#include <stdlib.h>

/* Super Ping))) Sensor

This sketch reads a PING))) ultrasonic rangefinder and returns the
distance to the closest object in range to a hundreth of an inch using a Due or Chipkit board.
Most stable at short distances.

The circuit:

  • +V connection of the PING))) attached to +5V
  • GND connection of the PING))) attached to ground
  • SIG connection of the PING))) attached to digital pin 7

http://www.arduino.cc/en/Tutorial/Ping

created 3 Nov 2008
by David A. Mellis
modified 30 Aug 2011
by Tom Igoe

modified to run on the Due at increased resolution
13 Feb 2013
Rick Dumouchelle

This example code is in the public domain.

*/

// this constant won’t change. It’s the pin number
// of the sensor’s output:
const int pingPin = 7;

void setup() {
// initialize serial communication:
Serial.begin(115200);
}

void loop()
{
// establish variables for duration of the ping,
// and the distance result in inches and centimeters:
float duration, inches, cm;

// The PING))) is triggered by a HIGH pulse of 2 or more microseconds.
// Give a short LOW pulse beforehand to ensure a clean HIGH pulse:
pinMode(pingPin, OUTPUT);
digitalWrite(pingPin, LOW);
delayMicroseconds(5);
digitalWrite(pingPin, HIGH);
delayMicroseconds(10);
digitalWrite(pingPin, LOW);

// The same pin is used to read the signal from the PING))): a HIGH
// pulse whose duration is the time (in microseconds) from the sending
// of the ping to the reception of its echo off of an object.
pinMode(pingPin, INPUT);
duration = pulseIn(pingPin, HIGH);
//conversions
inches = duration / 74 / 2;
cm = duration / 29 / 2;
if (inches <255 && inches >0 ){
Serial.print(inches);
Serial.print("in, ");
Serial.print(cm);
Serial.print(“cm”);
Serial.println();
delay(10);
}
}
[/code]