[Solved] 8*2 LCD Setup with Arduino?

Hello,

I’m resuming this post becouse i bought an LCD 16x2 LMB162ABC and I’m unable to run it in Arduino 21 (no data displayed).

Here’s the code:

[code]/*
LiquidCrystal Library - display() and noDisplay()

Demonstrates the use a 16x2 LCD display. The LiquidCrystal
library works with all LCD displays that are compatible with the
Hitachi HD44780 driver. There are many of them out there, and you
can usually tell them by the 16-pin interface.

This sketch prints “Hello World!” to the LCD and uses the
display() and noDisplay() functions to turn on and off
the display.

The circuit:

  • LCD RS pin to digital pin 12
  • LCD Enable pin to digital pin 11
  • LCD D4 pin to digital pin 5
  • LCD D5 pin to digital pin 4
  • LCD D6 pin to digital pin 3
  • LCD D7 pin to digital pin 2
  • 10K resistor:
  • ends to +5V and ground
  • wiper to LCD VO pin (pin 3)

Library originally added 18 Apr 2008
by David A. Mellis
library modified 5 Jul 2009
by Limor Fried (http://www.ladyada.net)
example added 9 Jul 2009
by Tom Igoe
modified 8 Feb 2010
by Tom Igoe

This example code is in the public domain.

http://www.arduino.cc/en/Tutorial/LiquidCrystal
*/

// include the library code:
#include <LiquidCrystal.h>

// initialize the library with the numbers of the interface pins
LiquidCrystal lcd(12, 11, 5, 4, 3, 2);

void setup() {
// set up the LCD’s number of columns and rows:
lcd.begin(8, 2);
// Print a message to the LCD.
lcd.print(“hello, world!”);
}

void loop() {
// Turn off the display:
lcd.noDisplay();
delay(500);
// Turn on the display:
lcd.display();
delay(500);
}[/code]

Onky the blinking display is working (from noDisplay() to display() ).
Ithink I’ve done a good work with solder and wires are correct, same as http://arduino.cc/en/Tutorial/LiquidCrystalDisplay

Thanks in advance!

Marco