Solar powered sensors for Home Assistant with XIAO MG24/nrf54l15

I like to share my examples of solar powered sensors (temperature, humidity, pressure) for Home Assistant using the BtHome protocol: XIAO MG24 (Arduino), XIAO nrf54l15 (nrf Connect)

Key features: with advertising interval of 15 seconds (i know, way to often for temperature, but this is my benchmark), the average current is ~40µA (MG24) and ~10µA (nrf54l15)

My diagnostic dashboard:


Comments:

  • Voltage derivative is a history-graph, others are statistics-graph with 5 minute average.That’s why voltage derivative shows a more noisy signal.
  • Packet loss is calculated based on a counter that increments with every sent packet. With some Home Assistant helpers (statistics, template) it’s easy to determine packet loss rate.
  • MG24 has a 5F/6V SuperCap, 54L15 a 1.5F/5.5V SuperCap
  • MG24 has a 6V 50mA solar panel with Z-diode to protect SuperCap
  • 54L15 has a 5V 30mA solar panel without Z-diode
  • All solar panels are not exposed to direct sunlight
3 Likes

Hi there,

Pretty cool , I’m liking those SuperCaps.. :+1:

HTH
GL :slight_smile: PJ :v: