Solar panel on solar shield V.2.2

Hi …

Yes … my mistake in typing … in fact it is Open circuit Voltage (Voc) which is 7.2V., So even if the “Voc” has a voltage slightly higher than 6V the panel can be used without risk and danger from SeedStudio Arduino Solar Shield V. 2.2?

Can you confirm it? Thanks for your help. :slight_smile: :slight_smile: :slight_smile: :slight_smile: