Set up connections between two BluetoothBee step by step

Hi,

I have problems connecting my Bee in Linux.
I tried to follow the guide from the wiki. So I can see it, and pair it. But I cannot open the rfcomm via cutecom. The error message didn’t really help. Is there another way I can try (maybe via commandline) to open the rfcomm device?
I also tried pairing via hcitool. It works too. But browsing the device with sdptool doesn’t show any services. Is that supposed to be that way?

I tried it with Windows and it worked. But it won’t help me with my Linux application :wink:

So has someone a suggestion?

Thank you in advance.

Best regards,