SenseCAP S2120 Firmware version 2.0 decoding errors

apparently so… this was an addition that I and i assume atleast one other person asked for… I just got 1.15 version to try like 2 days ago and it did not work for me so i had to roll back… i dont think the app and the dashboard have been updated… that is my assumption… my device would not transmit data after the upgrade… but if i went directly into the device via the app and direct bluethooth and commanded a reading it would return all the values to the app… via the bluetooth but something blocked the LoRa to send any readings to the cloud