SenseCAP M2 - The device doesn't join AWS IoT through the gateway

Hi, akira.

I would like to know the LoRa Log of the M2 gateway when your LoRaWAN device connects to AWS IoT through the M2 gateway(You can refer to the following image to check the LoRa Log)

Normally, the LoRa Log after the gateway receives a join request from a device will look like this.

Tue Dec  3 01:37:50 2024 daemon.info lora_pkt_fwd[4426]: INFO: [up] Join-Request from 2CF7F1C0543001D1
Tue Dec  3 01:37:50 2024 daemon.info lora_pkt_fwd[4426]:
Tue Dec  3 01:37:50 2024 daemon.info lora_pkt_fwd[4426]: JSON up: {"rxpk":[{"jver":1,"tmst":1402283206,"chan":0,"rfch":0,"freq":923.200000,"mid": 8,"stat":1,"modu":"LORA","datr":"SF10BW125","codr":"4/5","rssis":-40,"lsnr":14.0,"foff":211,"rssi":-39,"size":23,"data":"ACVigYp21vZ20QEwVMDx9yz5kcsQzcE="}]}

The gateway then receives a downlink message with the same spreading factor and bandwidth as the Join request message.

Tue Dec  3 01:37:51 2024 daemon.info lora_pkt_fwd[4426]: JSON down: {"txpk":{"imme":false,"rfch":0,"powe":14,"ant":0,"brd":0,"tmst":1407283206,"tmms":null,"freq":923.2,"modu":"LORA","datr":"SF10BW125","codr":"4/5","fdev":null,"ncrc":null,"ipol":true,"prea":null,"size":33,"data":"II4tz3Wi2sJ7+oH29YQoz/bfEGNQdRvNqLfq9GHkdcae"}}

What is known is that the initial configuration of the M2 gateway to the AWS IoT platform may have a delay of a few hours, during which time the device cannot connect and upload data properly.