Seeeduino Xiao PWM

Seeed Studio XIAO SAMD21 has 14 PINs, which can be used for 11 digital interfaces, 11 mock interfaces, 10 PWM interfaces (d1-d10), 1 DAC output pin D0, 1 SWD pad interface, 1 I2C interface, 1 SPI interface, 1 UART interface, Serial communication indicator (T/R), Blink light (L) through pin multiplexing. The colors of LEDs(Power,L,RX,TX) are green, yellow, blue and blue. Moreover, Seeed Studio XIAO SAMD21 has a Type-C interface which can supply power and download code. There are two reset button, you can short connect them to reset the board

I am not an expert but i think you are mixing analog and digital
try pin id as A1, A2, A3 etc, or D1, D2, D3 and dont mix analog and digital read write
you dont need to use the term ledPin as an interger try hard coding the pin as A1