I got stuck when compiling (this step: Use Arduino Borads as DAPLink Device | Seeed Studio Wiki)".
Settings and error message in the image. How can I solve this?
Complete message:
Arduino: 1.8.13 (Mac OS X), Board: “Seeeduino Zero, TinyUSB, Off”
/Users/harmvanvugt/Documents/Arduino/libraries/Seeed_Arduino_DAPLink-master/examples/simple_daplink/simple_daplink.ino: In function 'void setup()':
simple_daplink:101:13: error: 'class Adafruit_USBD_HID' has no member named 'setStringDescriptor'; did you mean 'setReportDescriptor'?
usb_hid.setStringDescriptor("CMSIS-DAP");
^~~~~~~~~~~~~~~~~~~
setReportDescriptor
/Users/harmvanvugt/Documents/Arduino/libraries/Seeed_Arduino_DAPLink-master/examples/simple_daplink/simple_daplink.ino: In function 'void loop()':
simple_daplink:128:17: error: 'class Adafruit_USBD_CDC' has no member named 'baud'
baud = Serial.baud();
^~~~
Multiple libraries were found for "Adafruit_TinyUSB.h"
Used: /Users/harmvanvugt/Documents/Arduino/libraries/Adafruit_TinyUSB_Arduino-master
Not used: /Users/harmvanvugt/Documents/Arduino/libraries/Adafruit_TinyUSB_Library
exit status 1
'class Adafruit_USBD_HID' has no member named 'setStringDescriptor'; did you mean 'setReportDescriptor'?
This report would have more information with
"Show verbose output during compilation"
option enabled in File -> Preferences.