Seeed Xiao ePaper Breakout Board and XIAO ESP32S3 and a GooDisplay 184x88 screen not working with GxEPD2_BW

Hi there,
Does this run?

#include <SPI.h>
//EPD
#include "Display_EPD_W21_spi.h"
#include "Display_EPD_W21.h"
#include "Ap_29demo.h"  


void setup() {
#ifdef ESP8266
   pinMode(D0, INPUT);  //BUSY
   pinMode(D1, OUTPUT); //RES 
   pinMode(D2, OUTPUT); //DC   
   pinMode(D4, OUTPUT); //CS     
#endif 
#ifdef Arduino_UNO
   pinMode(4, INPUT);  //BUSY
   pinMode(5, OUTPUT); //RES 
   pinMode(6, OUTPUT); //DC   
   pinMode(7, OUTPUT); //CS   
#endif 
   //SPI
   SPI.beginTransaction(SPISettings(10000000, MSBFIRST, SPI_MODE0)); 
   SPI.begin ();  
}

//Tips//
/*
1.Flickering is normal when EPD is performing a full screen update to clear ghosting from the previous image so to ensure better clarity and legibility for the new image.
2.There will be no flicker when EPD performs a partial refresh.
3.Please make sue that EPD enters sleep mode when refresh is completed and always leave the sleep mode command. Otherwise, this may result in a reduced lifespan of EPD.
4.Please refrain from inserting EPD to the FPC socket or unplugging it when the MCU is being powered to prevent potential damage.)
5.Re-initialization is required for every full screen update.
6.When porting the program, set the BUSY pin to input mode and other pins to output mode.
*/
void loop() {
   unsigned char i;
#if 1 //Full screen refresh, fast refresh, and partial refresh demostration.

      EPD_HW_Init(); //Full screen refresh initialization.
      EPD_WhiteScreen_White(); //Clear screen function.
      EPD_DeepSleep(); //Enter the sleep mode and please do not delete it, otherwise it will reduce the lifespan of the screen.
      delay(2000); //Delay for 2s. 
     /************Full display(2s)*******************/
      EPD_HW_Init(); //Full screen refresh initialization.
      EPD_WhiteScreen_ALL(gImage_1); //To Display one image using full screen refresh.
      EPD_DeepSleep(); //Enter the sleep mode and please do not delete it, otherwise it will reduce the lifespan of the screen.
      delay(2000); //Delay for 2s. 

  #if 1 //Partial refresh demostration.
  //Partial refresh demo support displaying a clock at 5 locations with 00:00.  If you need to perform partial refresh more than 5 locations, please use the feature of using partial refresh at the full screen demo.
  //After 5 partial refreshes, implement a full screen refresh to clear the ghosting caused by partial refreshes.
  //////////////////////Partial refresh time demo/////////////////////////////////////
      EPD_HW_Init(); //Electronic paper initialization. 
      EPD_SetRAMValue_BaseMap(gImage_basemap); //Please do not delete the background color function, otherwise it will cause unstable display during partial refresh.
      for(i=0;i<6;i++)
      EPD_Dis_Part_Time(32,56+24*0,Num[i],         //x-A,y-A,DATA-A
                        32,56+24*1,Num[0],         //x-B,y-B,DATA-B
                        32,56+24*2,gImage_numdot, //x-C,y-C,DATA-C
                        32,56+24*3,Num[0],        //x-D,y-D,DATA-D
                        32,56+24*4,Num[1],24,32); //x-E,y-E,DATA-E,Resolution 24*32
                        
      EPD_DeepSleep();  //Enter the sleep mode and please do not delete it, otherwise it will reduce the lifespan of the screen.
       delay(2000); //Delay for 2s. 
      EPD_HW_Init(); //Full screen refresh initialization.
      EPD_WhiteScreen_White(); //Clear screen function.
      EPD_DeepSleep(); //Enter the sleep mode and please do not delete it, otherwise it will reduce the lifespan of the screen.
       delay(2000); //Delay for 2s. 
  #endif  
  
  #if 0 //Demo of using partial refresh to update the full screen, to enable this feature, please change 0 to 1.
  //After 5 partial refreshes, implement a full screen refresh to clear the ghosting caused by partial refreshes.
  //////////////////////Partial refresh time demo/////////////////////////////////////
      EPD_HW_Init(); //E-paper initialization 
      EPD_SetRAMValue_BaseMap(gImage_p1); //Please do not delete the background color function, otherwise it will cause an unstable display during partial refresh.
      EPD_Dis_PartAll(gImage_p1); //Image 1
      EPD_Dis_PartAll(gImage_p2); //Image 2
      EPD_Dis_PartAll(gImage_p3); //Image 3
      EPD_Dis_PartAll(gImage_p4); //Image 4
      EPD_Dis_PartAll(gImage_p5); //Image 5 
      EPD_DeepSleep();//Enter the sleep mode and please do not delete it, otherwise it will reduce the lifespan of the screen.
      delay(2000); //Delay for 2s. 
      EPD_HW_Init(); //Full screen refresh initialization.
      EPD_WhiteScreen_White(); //Clear screen function.
      EPD_DeepSleep(); //Enter the sleep mode and please do not delete it, otherwise it will reduce the lifespan of the screen.
      delay(2000); //Delay for 2s. 
  #endif
  
  #if 0 //Demonstration of full screen refresh with 180-degree rotation, to enable this feature, please change 0 to 1.
      /************Full display(2s)*******************/
      EPD_HW_Init_180(); //Full screen refresh initialization.
      EPD_WhiteScreen_ALL(gImage_1); //To Display one image using full screen refresh.
      EPD_DeepSleep(); //Enter the sleep mode and please do not delete it, otherwise it will reduce the lifespan of the screen.
      delay(2000); //Delay for 2s. 
  #endif        
  
#endif

#ifdef ESP8266
  while(1) 
    {
     Sys_run();//System run
     LED_run();//Breathing lamp
    }
#endif
#ifdef Arduino_UNO
 while(1);  // The program stops here   
#endif
}

GL :slight_smile: PJ
:v:

from here?
GDEM0097T61_Arduino.zip (11.6 KB)