Thanks but it’s not there. I am looking for a component I can import in Fusion 360 (or any other similar software) that can be used to place in a schematic which can then be used to generate a Gerber file to print a custom PCB. These components are very standard and ubiquitous. There’s a public library accessible in Fusion 360 called “Seeed Studio XIAO Series” that has the XIAO ESP32C3 but not the ESP32C6.
I emailed Seeed Support with this query “In Fusion 360 electronics design there is a library called “Seeed Studio XIAO Series” and they have the component for the ESP32C3 but not the ESP32C6. Can you please update this library ASAP and add the component for the ESP32C6 as I need it to make my custom PCB. Thanks!”
and I got back this most ridiculous response:
"Hi, we can quote you for components even if they are not in our OPL.
As long as you write the correct MPN or SKU and the corresponding link in the BOM.
Please do not hesitate to contact us if you have further problems.
Best Regards,
Krystal
Seeed Fusion Support Team
So, @ Seeed_Harrison, the bottom line is the component for the XIAO ESP32C3 is there in the public library and it shouldn’t be very hard for the person from XIAO who uploaded that component to modify it for the C6 since the only changes are on the bottom. Is there anyone else I can reach out to? Thanks.