Seeed Studio XIAO ESP32C6

Hi there,
Actually Your’e half correct… LOL
If I may :man_bowing: The word “Xiao” in Chinese means Tiny. The Footprint was establish several years ago. They want to develop innovative ways to squeeze more into less… Sound familiar :smile:
To do it properly you need a cutout in the Board. The Battery Pads are the main point so, any extra I/O is gravy. The C6 and the S3 are so close in specs It’s just a matter of time before even further combinations show up from Espressif to blur the line even further.
They market the C6 as dual core , but no code for it exists, AFAIK.?
with only a 1uA in sleep difference between them, I’m going S3 unless I have to have the WiFi 6 stuff or Zigbee, matter etc.

S3 is more bang for the buc and a TRUE Dual core IMO. the PSram and more I/o via a connector is to easy to pass up. I’m banking on them combining or adding too in the future,
HTH
GL :slight_smile: PJ :v: