Seeduino Xiao and IR relay example in Arduino?

A challenge with the simple IR relay sketch from the Examples, and it’s not functioning as expected. I’ve checked the compatibility, ensured library dependencies are met, selected the correct port and board in the Arduino IDE, and confirmed that the XIAO board is receiving sufficient power. Despite these efforts, the sketch doesn’t seem to work as intended.