SD_Test problems

Hi @Hansen, I’m having a similar problem as reported in the discussion between @ansonhe97 and @blanee Using SD file access and WiFi in the same sketch on Wio Terminal, i.e. as soon as I include the AtWiFi library, access to the SD files is blocked. I think it’s the same problem, if so can you tell me about the resolution of this so that I can use the new FS library the previous one was giving me problems opening two subsequent files. So now I’m stuck if I put the previous one does not work if I put the recent one another does not work.
I look forward to the resolution