SD_Test problems

Click to see the code
/*
Connect the SD card to the following pins:
SD card attached to SPI bus as follows:
** MOSI - pin 11
** MISO - pin 12
** CLK - pin 13
** CS - pin 4 (for MKRZero SD: SDCARD_SS_PIN)
*/

#include <Seeed_FS.h>
//#undef USESPIFLASH
#define USESPIFLASH
#ifdef USESPIFLASH
#define DEV SPIFLASH
#include “SFUD/Seeed_SFUD.h”
#else
#define DEV SD
#include “SD/Seeed_SD.h”
#endif

#define SERIAL Serial

#ifdef SAMD21
#define SDCARD_SS_PIN 1
#define SDCARD_SPI SPI
#endif
int c = 0;

void listDir(fs::FS &fs, const char *dirname, uint8_t levels)
{
SERIAL.print("Listing directory: ");
SERIAL.println(dirname);

File root = fs.open(dirname);
if (!root)
{
    SERIAL.println("Failed to open directory");
    return;
}
if (!root.isDirectory())
{
    SERIAL.println("Not a directory");
    return;
}

File file = root.openNextFile();
while (file)
{
    if (file.isDirectory())
    {
        SERIAL.print("  DIR : ");
        SERIAL.println(file.name());
        if (levels)
        {
            listDir(fs, file.name(), levels - 1);
        }
    }
    else
    {
        SERIAL.print("  FILE: ");
        SERIAL.print(file.name());
        SERIAL.print("  SIZE: ");
        SERIAL.println(file.size());
    }
    file = root.openNextFile();
}

}

void createDir(fs::FS &fs, const char *path)
{
SERIAL.print("Creating Dir: ");
SERIAL.println(path);
if (fs.mkdir(path))
{
SERIAL.println(“Dir created”);
}
else
{
SERIAL.println(“mkdir failed”);
}
}

void removeDir(fs::FS &fs, const char *path)
{
SERIAL.print("Removing Dir: ");
SERIAL.println(path);
if (fs.rmdir(path))
{
SERIAL.println(“Dir removed”);
}
else
{
SERIAL.println(“rmdir failed”);
}
}

void readFile(fs::FS &fs, const char *path)
{
SERIAL.print("Reading Dir: ");
SERIAL.println(path);
File file = fs.open(path);
if (!file)
{
SERIAL.println(“Failed to open file for reading”);
return;
}

SERIAL.println("Read from file: ");
while (file.available())
{
    SERIAL.write(file.read());
}
file.close();

}

void writeFile(fs::FS &fs, const char *path, const char *message)
{
SERIAL.print("Writing file: ");
SERIAL.println(path);
File file = fs.open(path, FILE_WRITE);
if (!file)
{
SERIAL.println(“Failed to open file for writing”);
return;
}

if (file.print(message))
{
    SERIAL.println("File written");
}
else
{
    SERIAL.println("Write failed");
}

file.close();

}

void appendFile(fs::FS &fs, const char *path, const char *message)
{
SERIAL.print("Appending to file: ");
SERIAL.println(path);

File file = fs.open(path, FILE_APPEND);
if (!file)
{
    SERIAL.println("Failed to open file for appending");
    return;
}
if (file.print(message))
{
    SERIAL.println("Message appended");
}
else
{
    SERIAL.println("Append failed");
}
file.close();

}

void renameFile(fs::FS &fs, const char *path1, const char *path2)
{
SERIAL.print("Renaming file “);
SERIAL.print(path1);
SERIAL.print(” to ");
SERIAL.println(path2);
if (fs.rename(path1, path2))
{
SERIAL.println(“File renamed”);
}
else
{
SERIAL.println(“Rename failed”);
}
}

void deleteFile(fs::FS &fs, const char *path)
{
SERIAL.print("Deleting file: ");
SERIAL.println(path);
if (fs.remove(path))
{
SERIAL.println(“File deleted”);
}
else
{
SERIAL.println(“Delete failed”);
}
}

void testFileIO(fs::FS &fs, const char *path)
{
File file = fs.open(path);
static uint8_t buf[512];
size_t len = 0;
uint32_t start = micros();
uint32_t end = start;
if (file)
{
len = file.size();
size_t flen = len;
start = micros();
while (len)
{
size_t toRead = len;
if (toRead > 512)
{
toRead = 512;
}
file.read(buf, toRead);
len -= toRead;
}
end = micros() - start;
SERIAL.print(flen);
SERIAL.print(" bytes read for “);
SERIAL.print(end);
SERIAL.println(” ns");
file.close();
}
else
{
SERIAL.println(“Failed to open file for reading”);
}
}

void setup()
{
SERIAL.begin(115200);
pinMode(5, OUTPUT);
digitalWrite(5, HIGH);
while (!SERIAL)
{
};
#ifdef SFUD_USING_QSPI
while (!DEV.begin(104000000UL))
{
SERIAL.println(“Card Mount Failed”);
return;
}
#else
while (!DEV.begin(SDCARD_SS_PIN, SDCARD_SPI, 4000000UL))
{
SERIAL.println(“Card Mount Failed”);
return;
}
#endif

#ifdef USESPIFLASH
uint8_t flashType = DEV.flashType();
if (flashType == FLASH_NONE)
{
SERIAL.println(“No SD card attached”);
return;
}
#else
uint8_t cardType = DEV.cardType();
if (cardType == CARD_NONE)
{
SERIAL.println(“No SD card attached”);
return;
}
#endif

#ifdef USESPIFLASH
uint8_t flashSize = DEV.flashSize() / (1024 * 1024);
SERIAL.print("SD Card Size: ");
SERIAL.print((uint32_t)flashSize);
SERIAL.println(“MB”);
#else
uint64_t cardSize = DEV.cardSize() / (1024 * 1024);
SERIAL.print("SD Card Size: ");
SERIAL.print((uint32_t)cardSize);
SERIAL.println(“MB”);
#endif
}

void loop()
{
c++;
delay(3000);
SERIAL.println©;
readFile(DEV, “/cfg2.json”);
readFile(DEV, “/cfg3.json”);
deleteFile(DEV, “/cfg2.json”);
writeFile(DEV, “/cfg2.json”, “file2!!!\n”);
readFile(DEV, “/cfg2.json”);
delay(1000);
deleteFile(DEV, “/cfg3.json”);
writeFile(DEV, “/cfg3.json”, “file3!!!\n”);
readFile(DEV, “/cfg3.json”);
}

tip : If you have large code chunks (or logs) , you can collapse (and format) them to avoid a very long post like this :

[details=Click to see the code]
```cpp

code here

[/details]