Changed the code like this, still shows SD FAILED:
#include <Arduino.h>
#include <TFT_eSPI.h>
#include <SPI.h>
#include <Wire.h>
#include <Adafruit_Sensor.h>
#include "Adafruit_BME680.h"
#include <SD.h>
#define SEALEVELPRESSURE_HPA (1013.25)
#if defined(CONFIG_IDF_TARGET_ESP32S3) || defined(CONFIG_IDF_TARGET_ESP32C3)
#include "esp_wifi.h"
#include "WiFi.h"
const char *ntpServer = "time.cloudflare.com";
const char *ssid = "Adith";
const char *password = "aadithsp";
#endif
#include "I2C_BM8563.h"
#include "NotoSansBold15.h"
I2C_BM8563 rtc(I2C_BM8563_DEFAULT_ADDRESS, Wire);
I2C_BM8563_TimeTypeDef timeStruct;
I2C_BM8563_DateTypeDef dateStruct;
Adafruit_BME680 bme; // Create a BME680 sensor object for I2C
TFT_eSPI tft = TFT_eSPI(); // Invoke library, pins defined in User_Setup.h
TFT_eSprite face = TFT_eSprite(&tft);
File myFile;
#define CLOCK_X_POS 10
#define CLOCK_Y_POS 10
#define CLOCK_FG TFT_SKYBLUE
#define CLOCK_BG TFT_NAVY
#define SECCOND_FG TFT_RED
#define LABEL_FG TFT_GOLD
#define CLOCK_R 230.0f / 2.0f // Clock face radius (float type)
#define H_HAND_LENGTH CLOCK_R / 2.0f
#define M_HAND_LENGTH CLOCK_R / 1.4f
#define S_HAND_LENGTH CLOCK_R / 1.3f
#define FACE_W CLOCK_R * 2 + 1
#define FACE_H CLOCK_R * 2 + 1
// Calculate 1 second increment angles. Hours and minute hand angles
// change every second so we see smooth sub-pixel movement
#define SECOND_ANGLE 360.0 / 60.0
#define MINUTE_ANGLE SECOND_ANGLE / 60.0
#define HOUR_ANGLE MINUTE_ANGLE / 12.0
// Sprite width and height
#define FACE_W CLOCK_R * 2 + 1
#define FACE_H CLOCK_R * 2 + 1
// Time h:m:s
uint8_t h = 0, m = 0, s = 0;
float time_secs = h * 3600 + m * 60 + s;
// Time for next tick
uint32_t targetTime = 0;
int memory_status = 0;
// =========================================================================
// Setup
// =========================================================================
void setup() {
Serial.begin(19200);
while (!Serial);
Serial.println("Booting...");
// Initialise the screen
tft.init();
// Ideally set orientation for good viewing angle range because
// the anti-aliasing effectiveness varies with screen viewing angle
// Usually this is when screen ribbon connector is at the bottom
tft.setRotation(0);
tft.fillScreen(TFT_BLACK);
// Create the clock face sprite
//face.setColorDepth(8); // 8 bit will work, but reduces effectiveness of anti-aliasing
face.createSprite(FACE_W, FACE_H);
// Only 1 font used in the sprite, so can remain loaded
face.loadFont(NotoSansBold15);
// Draw the whole clock - NTP time not available yet
renderFace(time_secs);
#if defined(CONFIG_IDF_TARGET_ESP32S3) || defined(CONFIG_IDF_TARGET_ESP32C3)
WiFi.begin(ssid, password);
for (int a = 0; a < 10; a++) {
if (WiFi.status() != WL_CONNECTED) {
delay(500);
Serial.print("\nWaiting for WiFi Connection...");
}
delay(500);
}
delay(1000);
if (WiFi.status() == WL_CONNECTED) {
Serial.print("\nWiFi Successfully Connected!");
} else {
Serial.print("\nWiFi Connection Failed");
}
configTime(8 * 3600, 0, ntpServer);
struct tm timeInfo;
if (getLocalTime(&timeInfo)) {
timeStruct.hours = timeInfo.tm_hour;
timeStruct.minutes = timeInfo.tm_min;
timeStruct.seconds = timeInfo.tm_sec;
rtc.setTime(&timeStruct);
// dateStruct.weekDay = timeInfo.tm_wday;
// dateStruct.month = timeInfo.tm_mon + 1;
// dateStruct.date = timeInfo.tm_mday;
// dateStruct.year = timeInfo.tm_year + 1900;
// rtc.setDate(&dateStruct);
}
#endif
Wire.begin();
rtc.begin();
syncTime();
////////////////////////////////////////////////////////sensor and sd card
// while (!Serial)
// ;
Serial.println(F("\nBME688 test"));
//delay(1000);
if (!bme.begin()) {
Serial.println("\nCould not find a valid BME688 sensor, check wiring!");
while (1)
; // Stay in a loop if the sensor is not found
}
// Configure sensor settings
bme.setTemperatureOversampling(BME680_OS_8X);
bme.setHumidityOversampling(BME680_OS_2X);
bme.setPressureOversampling(BME680_OS_4X);
bme.setIIRFilterSize(BME680_FILTER_SIZE_3);
bme.setGasHeater(320, 150); // 320°C for 150 ms
///////////////////////////////////////////////////////////////////
// Open serial communications and wait for port to open:
// while (!Serial)
// ;
Serial.print("Initializing SD card... \n");
pinMode(D2, OUTPUT);
if (!SD.begin(D2)) {
Serial.println("initialization failed! \n");
memory_status = 0;
return;
}
Serial.println("initialization done.");
memory_status = 1;
}
// =========================================================================
// Loop
// =========================================================================
void loop() {
callfunction();
// Update time periodically
if (targetTime < millis()) {
// Update next tick time in 100 milliseconds for smooth movement
targetTime = millis() + 100;
// Increment time by 100 milliseconds
time_secs += 0.100;
// Midnight roll-over
if (time_secs >= (60 * 60 * 24)) time_secs = 0;
// All graphics are drawn in sprite to stop flicker
renderFace(time_secs);
// syncTime();
}
}
// =========================================================================
//call function
// =========================================================================
void callfunction() {
//////////////////////////////////////////////////////rtc function
I2C_BM8563_DateTypeDef dateStruct;
I2C_BM8563_TimeTypeDef timeStruct;
// Get RTC
rtc.getDate(&dateStruct);
rtc.getTime(&timeStruct);
// Print RTC
#if defined(CONFIG_IDF_TARGET_ESP32S3) || defined(CONFIG_IDF_TARGET_ESP32C3)
Serial.printf("%04d/%02d/%02d %02d:%02d:%02d\n",
dateStruct.year,
dateStruct.month,
dateStruct.date,
timeStruct.hours,
timeStruct.minutes,
timeStruct.seconds);
#endif
delay(0);
/////////////////////////////////////////////sensor function
if (!bme.performReading()) {
//Serial.println("Failed to perform reading :(");
return;
}
Serial.print("Temperature = " + String(bme.temperature) + "°C \n");
Serial.print("Humidity = " + String(bme.humidity) + "% \n");
Serial.print("Gas = " + String(bme.gas_resistance / 1000.0) + "KOhms \n");
//////////////////////////////////////////////////// sd card write function
if (memory_status == 1) {
myFile = SD.open("/test.txt", FILE_WRITE);
// if the file opened okay, write to it:
if (myFile) {
Serial.print("Writing to test.txt... \n");
myFile.println(dateStruct.year);
myFile.println(dateStruct.month);
myFile.println(dateStruct.date);
myFile.println(timeStruct.hours);
myFile.println(timeStruct.minutes);
myFile.println(timeStruct.seconds);
// close the file:
myFile.close();
Serial.println("Time Sensor done. \n");
} else {
// if the file didn't open, print an error:
Serial.println("error opening test.txt");
}
} else {
Serial.print("SD Failed \n");
}
// // re-open the file for reading:
// myFile = SD.open("/test.txt");
// if (myFile) {
// Serial.println("test.txt:");
// // read from the file until there's nothing else in it:
// while (myFile.available()) {
// Serial.write(myFile.read());
// }
// // close the file:
// myFile.close();
// } else {
// // if the file didn't open, print an error:
// Serial.println("error opening test.txt");
// }
}
// =========================================================================
// Draw the clock face in the sprite
// =========================================================================
static void renderFace(float t) {
float h_angle = t * HOUR_ANGLE;
float m_angle = t * MINUTE_ANGLE;
float s_angle = t * SECOND_ANGLE;
// The face is completely redrawn - this can be done quickly
face.fillSprite(TFT_BLACK);
// Draw the face circle
face.fillSmoothCircle(CLOCK_R, CLOCK_R, CLOCK_R, CLOCK_BG);
// Set text datum to middle centre and the colour
face.setTextDatum(MC_DATUM);
// The background colour will be read during the character rendering
face.setTextColor(CLOCK_FG, CLOCK_BG);
// Text offset adjustment
constexpr uint32_t dialOffset = CLOCK_R - 10;
float xp = 0.0, yp = 0.0; // Use float pixel position for smooth AA motion
// Draw digits around clock perimeter
for (uint32_t h = 1; h <= 12; h++) {
getCoord(CLOCK_R, CLOCK_R, &xp, &yp, dialOffset, h * 360.0 / 12);
face.drawNumber(h, xp, 2 + yp);
}
// Add text (could be digital time...)
face.setTextColor(LABEL_FG, CLOCK_BG);
face.drawString("DePaul", CLOCK_R, CLOCK_R * 0.75);
// Draw minute hand
getCoord(CLOCK_R, CLOCK_R, &xp, &yp, M_HAND_LENGTH, m_angle);
face.drawWideLine(CLOCK_R, CLOCK_R, xp, yp, 6.0f, CLOCK_FG);
face.drawWideLine(CLOCK_R, CLOCK_R, xp, yp, 2.0f, CLOCK_BG);
// Draw hour hand
getCoord(CLOCK_R, CLOCK_R, &xp, &yp, H_HAND_LENGTH, h_angle);
face.drawWideLine(CLOCK_R, CLOCK_R, xp, yp, 6.0f, CLOCK_FG);
face.drawWideLine(CLOCK_R, CLOCK_R, xp, yp, 2.0f, CLOCK_BG);
// Draw the central pivot circle
face.fillSmoothCircle(CLOCK_R, CLOCK_R, 4, CLOCK_FG);
// Draw cecond hand
getCoord(CLOCK_R, CLOCK_R, &xp, &yp, S_HAND_LENGTH, s_angle);
face.drawWedgeLine(CLOCK_R, CLOCK_R, xp, yp, 2.5, 1.0, SECCOND_FG);
face.pushSprite(5, 5, TFT_TRANSPARENT);
}
// =========================================================================
// Get coordinates of end of a line, pivot at x,y, length r, angle a
// =========================================================================
// Coordinates are returned to caller via the xp and yp pointers
#define DEG2RAD 0.0174532925
void getCoord(int16_t x, int16_t y, float *xp, float *yp, int16_t r, float a) {
float sx1 = cos((a - 90) * DEG2RAD);
float sy1 = sin((a - 90) * DEG2RAD);
*xp = sx1 * r + x;
*yp = sy1 * r + y;
}
void syncTime(void) {
targetTime = millis() + 100;
rtc.getTime(&timeStruct);
time_secs = timeStruct.hours * 3600 + timeStruct.minutes * 60 + timeStruct.seconds;
}