SD not initializing in XIAO RoundDisplay with ESP32C3

Hi there,
Start with this, Keeping in mind the only differences are the LIBs or the other stuff the load as “dependant” Ring any Bells?
So make a folder on your SD card called gif
copy the ‘monkeywink.gif’ to it.
Load the bin (any ESP flash tool will do) , press reset.
If that works you can try the Depaul_target.bin and see if it works for you as well,note I left the to edits in place. also, but you do need to plug in usb port for serial and for your code run.

HTH
GL :slight_smile: PJ
:sleeping:
GifViewer_target.zip (2.2 MB)
DePaul_target.zip (521.2 KB)

lmk when they work , I’ll show you in the morning after church later today where you may have gone wrong.