RFBee wireless sensor node

Hi,

I am doing some test with this configuration:
1 RFBee connected to PC (modem sketch)
1 RFBee on Xbee Carrier and DHT22 sensor (sign pin connected to D6 - thmphumpress sketch)
It’s my first “game” based on RFBee and probably something is not configured well.
I do not made any changes to the original sketches (only configure DHT 22 in sensor.h) but the system do not work correctly.

Sometimes on the serial console of Arduino IDE the system give me back as result only the Modem Ready message. I can set the command mode. No other AT command are accepted. Sometimes it seems start correctly and I have as result some hex strings.

I am also testing the Swapdmt but the python program seems not able to communicate with modem and devices.

What about your experiences ?
Any advices ?

Thanks
emkant